Technical FAQs

Ask a Question

Is there a handle lock for either a QO or HOM tandem breaker?

Issue:
Is there a handle lock for either a QO or HOM tandem breaker?

Product Line:
QO and HOM Tandem breakers

Environment:
This applies to QO and HOM Tandem breakers only.

Cause:
Want to be able to padlock a tandem breaker in the ON or OFF position.

Resolution:
The padlock attachment for the QO tandem breaker to lock 2 side by side tandem breakers in either the ON or OFF position is QOTHPA.
No padlock attachment is available for the HOM tandem breakers.


CTA-ID : 2050119
Was this helpful?
What can we do to improve the information ?