Technical FAQs

Ask a Question

What are the replacement parts for UFP222RGFI, Series G02, AC Disconnect?

Issue:
Product design repair parts

Product Line:
Air Conditioner Disconnect

Environment:
repair parts

Cause:
Maintenance

Resolution:
THE SQUARE D AC DISCONNECTS HAVE BEEN OBSOLETE SINCE ABOUT 2008 AND THERE ARE NO REPAIR PARTS AVAILABLE ANYMORE.

Only the parts listed below are considered field replaceable (for pictures see attached link):
Interior Trim - Cannot be provided due to UL labeling issues.
Pullout - 4050711750 (This pullout will work for either Series G01 or G02) PULLOUT IS OBSOLETE, NLA, NO REPLACEMENT
Interior Trim Mounting Screw 4020513001K (This kit includes 10 screws. Only one screw is required)
Receptacle - Purchase locally, Leviton #8899-G or 8899-I or equivalent (NEMA 5-20R, 125V, 20A, 2 Pole, 3 Wire Grounding, GFCI Duplex)
Receptacle Mounting Screws (2) - Purchase locally, 6-32 x .375 Machine Screw
Receptacle Mounting Nuts (2) - Purchase locally, 6-32 Hex Nut


 
Was this helpful?
What can we do to improve the information ?