Technical FAQs

Ask a Question

What are the electrical contact ratings on a float switch such as p/n 9036FG30?

Product Line:
 
9036 Float Switches  

Resolution:
 
These ratings are found in Digest 172, page 20-28.

For this example:

Ratings: Single Phase...2 HP@ 120 VAC......3 HP @ 240 VAC
: Poly phase......3 HP@ 120 VAC......5 HP@ 240 VAC

Voltage: 120/ 240 VAC.

obsolate new Res 2020542 per the CIC GMR


CTA-ID : 2049892
Was this helpful?
What can we do to improve the information ?