Technical FAQs

Ask a Question

What is the interrupting rating for a FH breaker at 600V?

Issue:
What is the interrupting rating for a FH breaker at 600V?

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
FH breaker is rated for 18K AIR at 600 Vac.


CTA-ID : 2050531
Was this helpful?
What can we do to improve the information ?