Technical FAQs

Ask a Question

What can be used in place of the Obsolete UFP222RD, for an air conditioning disconnect with an integral duplex receptacle?

Issue:
Product Design Features

Product Line:
AC Disconnect and Enclosed Molded Case Switches

Environment:
Duplex Receptacles

Cause:
Application

Resolution:
The AC Disconnects UFP and FP devices that contained a Duplex Receptacle have been obsolete since around 2008 and Square D will no longer offer any AC Disconnect or Enclosed Molded Case Switches, with an integral Duplex Receptacle. Consider using a QO200TR in conjunction with a Duplex Receptacle separately mounted in a rainproof enclosure.


CTA-ID : 2050605
Was this helpful?
What can we do to improve the information ?