Technical FAQs

Ask a Question

Does the CH321NRB accept Class J fuses?

Issue:
Fuse Type

Product Line:
Heavy Duty Safety Switches

Environment:
Class J fuses

Cause:
Application

Resolution:
No, It will no. If Class J fuses are required, consider using a 600V safety switch, CH361RB. Order neutral assembly CSN03 separately, if required.


CTA-ID : 2051151
Was this helpful?
What can we do to improve the information ?