Technical FAQs

Ask a Question

What size is the switch/fuse viewing window for the 5/15kV HVL switch enclosure? How high is it from the floor?

Issue:
What size is the switch/fuse viewing window for the 5/15kV HVL  switch enclosure?  How high is it from the floor?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The viewing window is 5.5`` high and 21.5`` wide. The center line of the window is 67.5`` from the floor for indoor. Add 4`` for NEMA 3R base channel. For inverted switches the center line of the window is 41`` from the floor for indoor. Add 4`` for NEMA 3R base channel. Revised 01/14/09.


CTA-ID : 2051435
Was this helpful?
What can we do to improve the information ?