Technical FAQs

Ask a Question

GV3ME80: How do you remove this device or take it off the DIN track?

Product Line:
GV3 GV2 manual motor starter IEC

Resolution:
There are two springs in the top back portion of the device that you push down and at the same pull the bottom of the starter away from the track.


CTA-ID : 2051311
Was this helpful?
What can we do to improve the information ?