Technical FAQs

Ask a Question

Is there a low consumption DC coil for Everlink D-Line Contactors?

No, the DC coils for the Everlink or LC1D**A contactors have a lower consumption than the older DC coils. The inrush is 19W and sealed is 7.5W. Average consumption on DC coils for Non Everlink LC1D40 to LC1D65 D-Line contactors was 22W

CTA-ID : 2051517
Was this helpful?
What can we do to improve the information ?