Technical FAQs

Ask a Question

When ordering a QEDS or QED2 switchboard with a Bolt Loc main fusible switch, are fuses included? What type of fuses should bn used on a Bolt Loc Switch?

Main fuses are not provided with the Bolt Loc switch as standard but are available as an option at the time the switchboard is ordered. A Bolt Loc switch uses a Class ``L`` fuse.


 
Was this helpful?
What can we do to improve the information ?