Technical FAQs

Ask a Question

Can H or J frame breakers be factory installed with control wire terminals?

Issue:
Can H or J frame breakers be factory installed with control wire terminals?

Product Line:
Powerpact H and J frame

Environment:
Products sold in North America

Cause:
Need control wire on a Powerpact H or J frame.

Resolution:
Yes, suffix LV for control wire taps on OFF end only; suffix LW for both ends.
They are also available as a field-installed accessory:
  • Control Wire Terminal for H-frame lug kit S37423
  • Control Wire Terminal for J-frame lug kit S37424

Each control-wire terminal has a 1/4 in. (6.3mm) male spade connector tab which allows monitoring of circuit status.
They may be used with wire sizes suitable for UL Listed insulated 1/4 in. female connectors.


 
Was this helpful?
What can we do to improve the information ?