Technical FAQs

Ask a Question

What does the second S indicate in part number 8536SCO3S?

Issue:     
Identifying forms and options in a NEMA starter part number

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Identifying forms and options in a NEMA starter

Resolution:
It can indicate either a separate source control circuit ( Form S) or a special starter used as a component in a reduced voltage starter or in a two speed starter.


CTA-ID : 2051276
Was this helpful?
What can we do to improve the information ?