Technical FAQs

Ask a Question

Is there a flashing 24 volt light module in the XB4 line for use with pilot lights and illuminated operators?

Issue:
Is there a flashing 24 volt light module in the XB4 line for use with pilot lights and illuminated operators?

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 Harmony 22mm Push Buttons

Cause:
Determine if a 22mm pilot light will work for their application.         
                           
Resolution:                                                                 
The part number for protected LED flashing light modules: for 24Vac/Vdc flashing is ZB4BV18B* for 110Vac flashing is ZB4BV18G*. * add suffix (1-White, 3 -Green, 4 - Red, 5-Yellow, 6-Blue).
 
Was this helpful?
What can we do to improve the information ?