Technical FAQs

Ask a Question

What is the difference between a: 3 pole, FDA and FA breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment
I Line (FDA and FA)

Resolution:
FDA breaker uses 3 inches in mounting height.
FA uses 4.5 inches in mounting height.
Both can be used in existing and new application I Line panels.


CTA-ID : 2050998
Was this helpful?
What can we do to improve the information ?