Technical FAQs

Ask a Question

Need a single phase 2p version of the Powerpact D and Powerpact L frame breaker?

Issue:
Is there a two pole version of the Powerpact D and Powerpact L frame breaker?

Product Lines:
Powerpact Breakers, Unit Mount and ILINE Breakers

Environment:
Products sold in North America

Cause:
Need a 2 pole breaker in the 400 A to 600A frame size.

Resolution:
The breaker only come in 3 and 4 pole versions, but the 3 pole breakers can be used in two pole applications just use the outer poles.

For more information on the Powerpact L frame consult PowerPact™ H-, J-, and L-Frame Circuit Breakers Catalog 0611CT1001.

The Powerpact D frame is currently being obsolete. The availability is limited.
 

Was this helpful?
What can we do to improve the information ?