Technical FAQs

Ask a Question

Do the Nema Contactors and Starters have dual hertz (50/60hz) rated coils?

No the Nema coils are not dual rated for 50/60 hertz. The 50 hertz and 60 hertz catalog number for the
coil may be the same. However, the lower frequency restricts the voltage capacity, for example: a 120v 60 hertz coil can only be used at 110-115v when used at 50 hertz.

CTA-ID : 2052312
Was this helpful?
What can we do to improve the information ?