Technical FAQs

Ask a Question

What is the difference between a HOMCGK2C and a HOMCGK2 Generator Interlock Kit?

Issue:
Product features

Product Line:
Generator Kits

Cause:
Accessory selection

Resolution:
Only difference is the packaging - the HOMCGK2C comes in a clam shell package designed for DIY market. There is no difference other than the packaging.
NOTE: As of 4Q/2015, the HOMCGK2 will be obsoleted when all stock is depleted and the HOMCGK2C will be offered instead. 


CTA-ID : 2051954
Was this helpful?
What can we do to improve the information ?