Technical FAQs

Ask a Question

What is the part number for a replacement external reset button for a size 3 starter with a melting alloy overload relay in a Nema 12 enclosure - 8536SEA?

Issue:     
Identifying part number for external reset button for an enclosed NEMA size 3 starters

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement reset button needed

Resolution:
The replacement external reset button is 30019-113-50; the replacement gasket is 29206-30700; the replacement ring nut is 30019-121-01.


CTA-ID : 2052665
Was this helpful?
What can we do to improve the information ?