Technical FAQs

Ask a Question

What is the numerical arc flash category for the NF panels? Are the categories listed on the panel labels?

Issue:
Panel arc flash category

Product Line:
Panelboards

Environment:
NF

Cause:
Rating and marking

Resolution:
The numerical arc flash category is not designated on the panel sticker. It must be established by an external authority and is not a part of the individual panel rating.


CTA-ID : 2052845
Was this helpful?
What can we do to improve the information ?