Technical FAQs

Ask a Question

What does the (3) designate in the part number LC1D123G7?

For spring termination versions, add (3) to the catalog number prior to adding the voltage code. (ex. LC1D12G7 becomes a LC1D123G7 or LC1D40AG7 becomes LC1D40A3G7). This applies only for the LC1D09 - LC1D65A contactors. Note: For the LC1D40A to D65A, the spring terminals are only on the control terminations and not on power terminations.

CTA-ID : 2053127
Was this helpful?
What can we do to improve the information ?