Technical FAQs

Ask a Question

Will a size 2, 8538 starter , with a 120V coil still work if only 100 volts is applied to it`s 120V coil?

All Square D NEMA rated Type S Starter coils are rated to operate between +10% to - 15 % of the coil`s normal operating voltage .


CTA-ID : 2053048
Was this helpful?
What can we do to improve the information ?