Technical FAQs

Ask a Question

Adding a CJL3300N to an existing CDP panel

The CJL3300N breaker is obsolete.
The Replacement breaker is a Square D LCL36300 breaker with a LCCMH mounting kit. These breakers are rated 35KAIC at 600V.

The LCCMH is a single breaker mounting kit. The CJL breaker could be double mounted, one mounted on each side of panel. Double mounting is no longer available with the LCCMH.



CTA-ID : 2053870
Was this helpful?
What can we do to improve the information ?