Technical FAQs

Ask a Question

Adding a CE3040B to an existing NHDP panel

The CE3040B breaker is obsolete, as are the CE3040E CE3040N and CE3040H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053877
Was this helpful?
What can we do to improve the information ?