Technical FAQs

Ask a Question

Adding a CE3070B to an existing NHDP panel

The CE3070B breaker is obsolete, as are the CE3070E CE3070N and CE3070H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053880
Was this helpful?
What can we do to improve the information ?