Technical FAQs

Ask a Question

Adding a CED or TED 125A 3 pole breaker to an existing Federal Pioneer CDP panel when original breaker part numbers are CED136125 or TED1306125.

The CED and TED breakers are obsolete.
The Replacement breaker is a Square D HDL36125 breaker with a HDCMH mounting kit. This breaker is rated 14KAIC at 600V to match existing.
The HDCMH will mount two H frame breakers.
An S37444 is included in the HDCMH to convert breaker from Lug-Lug to Lug-Pad. If a second breaker is being mounted on the HDCMH Hardware, order an additional S37444.
Hardware Kit requires both sides of panel and will only mount Powerpact H Breakers.

CTA-ID : 2053651
Was this helpful?
What can we do to improve the information ?