Technical FAQs

Ask a Question

When installing a SDSA3650 into a load center, must the leads be connected to a branch circuit breaker?

Issue:
When installing an SDSA3650 into a load center, must the leads be connected to a branch circuit breaker?

Product Line:
Surgelogic products sold and supported in the USA.

Environment:
Installation 

Cause:
Installation and Wiring

Resolution:
Connecting the SDSA3650 leads to a 3-pole, 15 - 30 ampere, branch circuit breaker is the recommended means of connection.


CTA-ID : 2053495
Was this helpful?
What can we do to improve the information ?