Technical FAQs

Ask a Question

Adding a CE3225N to an existing CDP panel

The CE3225N breaker is obsolete.
The Replacement breaker is a Square D JJL36225 breaker with a JDCMH mounting kit. This breaker is rated 25KAIC at 600V.
The JDCMH will mount two J frame breakers.
An S37445 is included in the JDCMH to convert breaker from Lug-Lug to Lug-Pad. If a second breaker is being mounted on the HDCMH Hardware, order an additional S37444.
Hardware Kit requires both sides of panel and will only mount Powerpact H Breakers.

CTA-ID : 2053668
Was this helpful?
What can we do to improve the information ?