Technical FAQs

Ask a Question

Can you use a GV3P starter ahead of (2) LC1D40-65 amp Contactors for a single phase, 240V reversing application?<br /><br />Does the GV3P have single phase sensitivity?

Product Line:

Tesys GV Manual Starter and Protectors
 
Resolution:
Yes, you can use the GV3P ahead of a reversing contactor pair. The answer to the second question also being yes, the GV3P will have to be wired so that the current flows through all three phases. This is done by wiring one of the 240V phases through L1, out T1 back up to L2 of the GV3P, out T2 of the GV3P to the contactor pair. Take the second 240V line on the GV3P straight through L3 to T3 and on to the reversing pair.


CTA-ID : 2052993
Was this helpful?
What can we do to improve the information ?