Technical FAQs

Ask a Question

Adding a CE1020E 20A 1 pole breaker to an existing CDP panel

The CE1020E breaker is obsolete.
Alternative breaker is an FFGP16020 with FFCMH mounting kit. Both breakers are rated at 18KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit. Only FF type breakers can mount on this hardware and it takes both sides of the panel.



CTA-ID : 2053894
Was this helpful?
What can we do to improve the information ?