Technical FAQs

Ask a Question

What is the largest amperage D Line IEC contactor that can accomodate spring terminals, using a ``3`` after the amperage in the part number, such as an LC1D123G7?

The ``3`` form for spring terminals is available on 65A and below IEC contactors. On the 40, 50 and 65 amp devices the spring terminals are on the control circuit only. It is not available on 80A, 115A or 150A D Line contactors.

CTA-ID : 2053331
Was this helpful?
What can we do to improve the information ?