Technical FAQs

Ask a Question

Adding a CE3060B to an existing NHDP panel

The CE3060B breaker is obsolete, as are the CE3060E CE3060N and CE3060H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053879
Was this helpful?
What can we do to improve the information ?