Technical FAQs

Ask a Question

Adding a CE3080B to an existing NHDP panel

The CE3080B breaker is obsolete, as are the CE3080E CE3080N and CE3080H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053881
Was this helpful?
What can we do to improve the information ?