Technical FAQs

Ask a Question

Adding a CE1020N 20A 1 pole breaker to an existing NHDP panel

The CE1020N breaker is obsolete.
Alternative breaker is an FFJP16020 with FF22NHDP mounting kit and MHMHDP mounting screws. Both breakers are rated at 25KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit.
This will mount in 22 inch wide NHDP panels only. They will not mount in the older 20 inch wide NHDP panels.



CTA-ID : 2053889
Was this helpful?
What can we do to improve the information ?