Technical FAQs

Ask a Question

Adding a CE1020N 15A 1 pole breaker to an existing CDP panel

The CE1020N breaker is obsolete.
Alternative breaker is an FFJP16020 with FFCMH mounting kit. Both breakers are rated at 25KAIC at 600V. Up to 6 FFGP breakers can mount on this hardware kit. Only FF type breakers can mount on this hardware and it takes both sides of the panel.



CTA-ID : 2053896
Was this helpful?
What can we do to improve the information ?