Technical FAQs

Ask a Question

Do the Type 316 stainless steel NEMA 4,4X,5 Heavy Duty safety switches with suffix SS have a gasket around the door?

Issue:
Product design

Product Line:
Heavy Duty Safety Switch

Environment:
Type 4/4X/5 switches

Cause:
Verification

Resolution:
Yes, they do have a gasket that is attached to the cover that presses against the enclosure to provide a watertight seal.


CTA-ID : 2053898
Was this helpful?
What can we do to improve the information ?