Technical FAQs

Ask a Question

Adding a CE3150B to an existing NHDP panel

The CE3150B breaker is obsolete, as are the CE3150E CE3150N and CE3150H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053874
Was this helpful?
What can we do to improve the information ?