Technical FAQs

Ask a Question

Adding a CE3020B to an existing NHDP panel

The CE3020B breaker is obsolete, as are the CE3020E CE3020N and CE3020H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053875
Was this helpful?
What can we do to improve the information ?