Technical FAQs

Ask a Question

Adding a CE3030B to an existing NHDP panel

The CE3030B breaker is obsolete, as are the CE3030E CE3030N and CE3030H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053876
Was this helpful?
What can we do to improve the information ?