Technical FAQs

Ask a Question

Adding a CE3100B to an existing NHDP panel

The CE3100B breaker is obsolete, as are the CE3100E CE3100N and CE3100H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053883
Was this helpful?
What can we do to improve the information ?