Technical FAQs

Ask a Question

Adding a CE30125B to an existing NHDP panel

The CE3125B breaker is obsolete, as are the CE3125E CE3125N and CE3125H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.

CTA-ID : 2053884
Was this helpful?
What can we do to improve the information ?