Technical FAQs

Ask a Question

Adding a CE3015B to an existing NHDP panel

The CE3015B breaker is obsolete, as are the CE3015E CE3015N and CE3015H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053885
Was this helpful?
What can we do to improve the information ?