Technical FAQs

Ask a Question

What are the dimensions for the M800S circuit breaker enclosure?

Issue:
Dimensions

Product Line:
Circuit Breaker Enclosure

Cause:
Dimensions

Resolution:
The M800R dimensions are: 40.38" H x 21.00" W x 9.75" D
Click this link for access to the Approval Drawing #3432
http://static.schneider-electric.us/docs/Circuit%20Protection/Circuit%20Breaker%20Enclosures/3432.pdf

The drawing is also attached for your reference. 


CTA-ID : 2053260
Was this helpful?
What can we do to improve the information ?