Technical FAQs

Ask a Question

What is the catalog number for auxiliary contacts for 8910DP contactors?

Product Line:
8910 Definite Pupose Contactors
Auxiliary contacts are not available for compact 8910DP contactors. If aux contacts are required, consider using an 8910DPA contactor which does have auxiliary contacts available.
The current Series C auxiliary contacts are 9999DD11: 1 NO and 1 NC, or 9999DD20: 2 NC, or 9999DD10: 1 NO, or 9999DD01: 1NC.

CTA-ID : 2053755
Was this helpful?
What can we do to improve the information ?