Technical FAQs

Ask a Question

What is the replacement coil part number for the LC1D09 through LC1D32 and LC1DT20 through LC1DT40 TeSys contactor?

Issue:
Identifying replacement coil for tesys D conactor

Product Line:
IEC Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Replacement coil is needed

Resolution:
DC replacement coils are not available.
AC Coils are 50/60 hertz for voltages as listed below:

Volts - Part Number
12 ____ LXD1J7
21 ____ LXD1Z7
24 ____ LXD1B7
32 ____ LXD1C7
36 ____ LXD1CC7
42 ____ LXD1D7
48 ____ LXD1E7
60 ____ LXD1EE7
100 ___ LXD1K7 ( never brought to North America )
110 ___ LXD1F7
115 ___ LXD1FE7
120 ___ LXD1G7
127 ___ LXD1FC7
200 ___ LXD1L7
208 ___ LXD1LE7
220 ___ LXD1M7
230 ___ LXD1P7
240 ___ LXD1U7
277 ___ LXD1W7
380 ___ LXD1Q7
400 ___ LXD1V7
415 ___ LXD1N7
440 ___ LXD1R7
480 ___ LXD1T7
575 ___ LXD1SC7
600 ___ LXD1X7
690 ___ LXD1Y7


Note: A contactor with an AC coil can be changed to a different AC voltage coil, IE you can take an LC1D09 with a 120VAC coil and put a 24VAC coil in it instead. An AC device cannot be switched to a DC coil, and a DC device cannot be switches to an AC coil. 
Was this helpful?
What can we do to improve the information ?