Technical FAQs

Ask a Question

Are auxiliary contacts available for 8965RO13?

Yes, order the 9999R10 for normally open or 9999R11 for normally closed. The contact blocks mount between the foward and reversing contactors. You can only install 1 contact block per 8965RO10 device. The 9999R blocks actually contain either 2 NO or 2 NC contacts in the module, one for each side of the device.


CTA-ID : 2053215
Was this helpful?
What can we do to improve the information ?