Technical FAQs

Ask a Question

What is the UL rating on a S29354 slide bar interlock?

Issue:
What is the UL rating on a S29354 slide bar interlock?

Product Line:
Circuit Breaker Accessory

Environment:
Standards

Cause:
Understanding the UL Listing of the S29354

Resolution:
The S29354 is a UL Listed Circuit Breaker Accessory in file E103955 Volume 3 Section 4.
This device is for mechanical interlock of any two side by side Powerpact H or J type circuit breakers.
 
Was this helpful?
What can we do to improve the information ?