Technical FAQs

Ask a Question

What is the replacement 208 volt coil for a Type SE, NEMA Size 3 contactor or starter?<br /><br />

For 2, 3, 4 and 5 pole devices the 208V 50/60Hz, replacement coil is a 31074-400-44, at 60 hertz.


CTA-ID : 2054420
Was this helpful?
What can we do to improve the information ?