Technical FAQs

Ask a Question

Where can the date code be found on both the QO and Homeline load centers?

Issue:
Product information features

Product Line:
QO and Homeline Load Centers

Environment:
Date codes

Cause:
Information

Resolution:

In ALL the current design QO and Homeline load centers, the date code can be found in one of three places;
1) On the outside Carton Label of the box, which is located at one of the ends of the carton.
ADD A SAMPLE CARTON LABEL

2) On the Box Label, which is located inside of the load center enclosure on either the left or right side wall and will be under the UL Mark of the label.(SEE ATTACHED AN EXAMPLE)
ADD A SAMPLE BOX LABEL

3) On the interior label, which is located on the black plastic material of the interior itself, near the Main Lugs of the load center.
 ADD A SAMPLE INTERIOR LABEL

The Date Code will read something like these examples below
1) 095231, (09=year, 52=week of the year, 3=day of week and 1=shift)
2) 171022 (17=year, 10=week of the year, 2=day of week and 2=shift)

For Older QO and Homeline load centers BEFORE the year 2000, the date code will read differently
FINISH EXPLAINING THIS




 
Was this helpful?
What can we do to improve the information ?