Technical FAQs

Ask a Question

What is the filler plate for the EDB, EGB, and EJB breakers?

Issue:  
What is the filler plate for the EDB, EGB, and EJB breakers?

Product line:  
NF Panelboards

Environment:  
Filler plates used to cover blank spaces Series 0 and Series E1

Cause:  
Need to know which filler plate to use.

Resolution:  
Use the NFFP15 filler plate kit (Qty 15), with Series E1 NF Interiors.  Use the EFP filler plates for the older Series 0 NF Panels.  The Series 0 NF Panels were manufactured up till Oct 2008, after which, the Series E1 NF panels were manufactured.
Was this helpful?
What can we do to improve the information ?