Technical FAQs

Ask a Question

Are the Powerpact H, J, and L breakers current limiting?


Issue:
Current limiting requirement

Product Line:
Circuit Breakers

Environment:
Applies to powerpact HJ/HL/HR,  JJ/JL/JR, and LJ/LL/LR.

Cause:
UL listed current limiting device.

Resolution:
PowerPact HJ/HL/HR, JJ/JL/JR and LJ/LL/LR frame circuit breakers are now labeled as current limiting with UL laboratories. The label on the front of the circuit breaker will identify this attribute.

Note:  Powerpact HD/HG, JD/JG and LD/LG circuit breakers do not carry the UL current limiting label.

For more information on the current limiting please refer to the Powerpact H/J/L catalog.

0611CT1001     Powerpact H/J/L Frame Catalog

Link to catalog:

http://static.schneider-electric.us/docs/Circuit%20Protection/Molded%20Case%20Circuit%20Breakers/0600%20A%20Frame%20PowerPact%20L/0611CT1001net.pdf

Technical Library:

http://products.schneider-electric.us/technical-library/


CTA-ID : 2054628
Was this helpful?
What can we do to improve the information ?